Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Field and Description |
---|---|
DegreesOfFreedomStatus |
DegreesOfFreedom.basePoint1Status
First rotation base point status.
|
DegreesOfFreedomStatus |
DegreesOfFreedom.basePoint2Status
Second rotation base point status.
|
static DegreesOfFreedomStatus |
DegreesOfFreedomStatus.FREE
The point or direction is under defined.
|
static DegreesOfFreedomStatus |
DegreesOfFreedomStatus.FREE_NORMAL
The direction represents a normal to two translational degrees of freedom.
|
static DegreesOfFreedomStatus |
DegreesOfFreedomStatus.INSTANTANEOUS
The point or direction is instantaneous.
|
static DegreesOfFreedomStatus |
DegreesOfFreedomStatus.INSTANTANEOUS_NORMAL
The direction represents a normal to two translational degrees of freedom.
|
static DegreesOfFreedomStatus |
DegreesOfFreedomStatus.NOT_USED
The field is not used.
|
DegreesOfFreedomStatus |
DegreesOfFreedom.rotationDirection1Status
First rotation direction status.
|
DegreesOfFreedomStatus |
DegreesOfFreedom.rotationDirection2Status
Second rotation direction status.
|
static DegreesOfFreedomStatus |
DegreesOfFreedomStatus.STATIC
The point or direction is well defined.
|
static DegreesOfFreedomStatus |
DegreesOfFreedomStatus.STATIC_NORMAL
The direction represents a normal to two translational degrees of freedom.
|
DegreesOfFreedomStatus |
DegreesOfFreedom.translationDirection1Status
First translation direction status.
|
DegreesOfFreedomStatus |
DegreesOfFreedom.translationDirection2Status
Second translation direction status.
|
Modifier and Type | Method and Description |
---|---|
static DegreesOfFreedomStatus |
DegreesOfFreedomStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DegreesOfFreedomStatus |
DegreesOfFreedomStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DegreesOfFreedomStatus[] |
DegreesOfFreedomStatus.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
DegreesOfFreedom(DegreesOfFreedomResult resultInitial,
int numRotationalInitial,
int numTranslationalInitial,
int numInstantaneousRotationalInitial,
int numInstantaneousTranslationalInitial,
DegreesOfFreedomStatus basePoint1StatusInitial,
Point3d basePoint1Initial,
DegreesOfFreedomStatus rotationDirection1StatusInitial,
Vector3d rotationDirection1Initial,
DegreesOfFreedomStatus basePoint2StatusInitial,
Point3d basePoint2Initial,
DegreesOfFreedomStatus rotationDirection2StatusInitial,
Vector3d rotationDirection2Initial,
DegreesOfFreedomStatus translationDirection1StatusInitial,
Vector3d translationDirection1Initial,
DegreesOfFreedomStatus translationDirection2StatusInitial,
Vector3d translationDirection2Initial)
Constructor for the DegreesOfFreedom object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.