Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Field and Description |
---|---|
static ComponentAssembly.CheckinCheckoutOption |
ComponentAssembly.CheckinCheckoutOption.BOTH
Checks in or Checks out the design element and its referenced source item
|
static ComponentAssembly.CheckinCheckoutOption |
ComponentAssembly.CheckinCheckoutOption.DEFAULT
Check In or Check Out option is determined by the system using whatever option is appropriate for the selected object type.
|
static ComponentAssembly.CheckinCheckoutOption |
ComponentAssembly.CheckinCheckoutOption.DESIGN_ELEMENT
Checks in or Checks out the design element
|
static ComponentAssembly.CheckinCheckoutOption |
ComponentAssembly.CheckinCheckoutOption.SOURCE_ITEM
Checks in or Checks out the source item that is referenced by a reuse design element or subordinate design element
|
Modifier and Type | Method and Description |
---|---|
static ComponentAssembly.CheckinCheckoutOption |
ComponentAssembly.CheckinCheckoutOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ComponentAssembly.CheckinCheckoutOption |
ComponentAssembly.CheckinCheckoutOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ComponentAssembly.CheckinCheckoutOption[] |
ComponentAssembly.CheckinCheckoutOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
ErrorList |
ComponentAssembly.checkinComponents(Component[] partOccs,
ComponentAssembly.CheckinCheckoutOption checkinInputOption)
Checks in array of components as per the option
ComponentAssembly.CheckinCheckoutOption . |
ErrorList |
ComponentAssembly.checkoutComponents(Component[] partOccs,
ComponentAssembly.CheckinCheckoutOption checkoutInputOption)
Checks out array of components as per the option
ComponentAssembly.CheckinCheckoutOption . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.