Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Field and Description |
---|---|
static ClearanceSet.ReanalyzePairCalculationMethod |
ClearanceSet.ReanalyzePairCalculationMethod.EXACT |
static ClearanceSet.ReanalyzePairCalculationMethod |
ClearanceSet.ReanalyzePairCalculationMethod.EXACT_IF_LOADED |
static ClearanceSet.ReanalyzePairCalculationMethod |
ClearanceSet.ReanalyzePairCalculationMethod.LIGHTWEIGHT |
static ClearanceSet.ReanalyzePairCalculationMethod |
ClearanceSet.ReanalyzePairCalculationMethod.USE_STORED_METHOD
Use the clearance set's defined analysis method.
|
Modifier and Type | Method and Description |
---|---|
static ClearanceSet.ReanalyzePairCalculationMethod |
ClearanceSet.ReanalyzePairCalculationMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ClearanceSet.ReanalyzePairCalculationMethod |
ClearanceSet.ReanalyzePairCalculationMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ClearanceSet.ReanalyzePairCalculationMethod[] |
ClearanceSet.ReanalyzePairCalculationMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ClearanceSet.reanalyzePairs(DisplayableObject[] firstObjects,
DisplayableObject[] secondObjects,
ClearanceSet.ReanalyzePairCalculationMethod calculationMethod)
Reanalyze a set of interferences using the specified analysis method.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.