public static class ClearanceSet.ReanalyzePairCalculationMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXACT |
static int |
_EXACT_IF_LOADED |
static int |
_LIGHTWEIGHT |
static int |
_USE_STORED_METHOD
Use the clearance set's defined analysis method.
|
static ClearanceSet.ReanalyzePairCalculationMethod |
EXACT |
static ClearanceSet.ReanalyzePairCalculationMethod |
EXACT_IF_LOADED |
static ClearanceSet.ReanalyzePairCalculationMethod |
LIGHTWEIGHT |
static ClearanceSet.ReanalyzePairCalculationMethod |
USE_STORED_METHOD
Use the clearance set's defined analysis method.
|
Modifier and Type | Method and Description |
---|---|
static ClearanceSet.ReanalyzePairCalculationMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ClearanceSet.ReanalyzePairCalculationMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ClearanceSet.ReanalyzePairCalculationMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final ClearanceSet.ReanalyzePairCalculationMethod USE_STORED_METHOD
public static final ClearanceSet.ReanalyzePairCalculationMethod LIGHTWEIGHT
public static final ClearanceSet.ReanalyzePairCalculationMethod EXACT_IF_LOADED
public static final ClearanceSet.ReanalyzePairCalculationMethod EXACT
public static final int _USE_STORED_METHOD
public static final int _LIGHTWEIGHT
public static final int _EXACT_IF_LOADED
public static final int _EXACT
public static ClearanceSet.ReanalyzePairCalculationMethod valueOf(int value)
public static ClearanceSet.ReanalyzePairCalculationMethod valueOf(String name)
public static ClearanceSet.ReanalyzePairCalculationMethod[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.