Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static TextJustification |
TextJustification.CENTER |
static TextJustification |
TextJustification.LEFT |
static TextJustification |
TextJustification.RIGHT |
Modifier and Type | Method and Description |
---|---|
TextJustification |
LetteringStyleBuilder.horizontalTextJustification()
Returns the horizontal text justification
License requirements: None. |
TextJustification |
LetteringPreferences.horizTextJust()
Returns the horizontal text justification
License requirements: None. |
static TextJustification |
TextJustification.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TextJustification |
TextJustification.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TextJustification[] |
TextJustification.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LetteringStyleBuilder.setHorizontalTextJustification(TextJustification horizontalTextJustification)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
LetteringPreferences.setHorizTextJust(TextJustification horizTextJust)
Sets the horizontal text justification
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.