Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static SymmetricalCenterlineBuilder.Types |
SymmetricalCenterlineBuilder.Types.FROM_FACE
Centerline from face
|
static SymmetricalCenterlineBuilder.Types |
SymmetricalCenterlineBuilder.Types.START_AND_END
Centerline from start and end point
|
Modifier and Type | Method and Description |
---|---|
SymmetricalCenterlineBuilder.Types |
SymmetricalCenterlineBuilder.type()
Returns the type of Symmetrical Centerline
License requirements: None. |
static SymmetricalCenterlineBuilder.Types |
SymmetricalCenterlineBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SymmetricalCenterlineBuilder.Types |
SymmetricalCenterlineBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SymmetricalCenterlineBuilder.Types[] |
SymmetricalCenterlineBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SymmetricalCenterlineBuilder.setType(SymmetricalCenterlineBuilder.Types type)
License requirements: drafting ("DRAFTING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.