Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static Symbol |
Symbol.BACKING
Specifies backing weld symbol (only one side of reference line )
|
static Symbol |
Symbol.BACKING_PLATE
Specifies backing plate weld symbol (GB only)
|
static Symbol |
Symbol.BEVEL_BUTT
Specifies bevel butt weld symbol
|
static Symbol |
Symbol.BEVEL_BUTT_BROAD_ROOT_FACE
Specifies bevel butt with broad root face weld symbol (ISO and DIN only)
|
static Symbol |
Symbol.BUTT_WITH_RAISED_EDGES
Specifies butt weld with raised edges
|
static Symbol |
Symbol.EDGE
Specifies edge weld symbol
|
static Symbol |
Symbol.FILLET
Specifies fillet weld symbol
|
static Symbol |
Symbol.FLARE_BEVEL
Specifies flare bevel weld symbol
|
static Symbol |
Symbol.FLARE_V
Specifies flare V weld symbol
|
static Symbol |
Symbol.FOLD_JOINT
Specifies fold joint weld symbol
(ISO and DIN only, only on one side of reference line)
|
static Symbol |
Symbol.INCLINED_JOINT
Specifies inclined joint weld symbol
|
static Symbol |
Symbol.INTERMITTENT
Specifies intermittent weld symbol (ESKD only)
|
static Symbol |
Symbol.JBUTT
Specifies J buttt weld symbol
|
static Symbol |
Symbol.LAST
Last enum value.
|
static Symbol |
Symbol.NONE
Speifies no weld symbol
|
static Symbol |
Symbol.NOT_SPECIFIED
Specifies weld symbol not specified
|
static Symbol |
Symbol.PLUG_SLOT
Specifies plug/slot weld symbol
|
static Symbol |
Symbol.SEAM
Specfies seam weld symbol
|
static Symbol |
Symbol.SINGLE_FLANGE
Specifiies single flange weld symbol (JIS only)
|
static Symbol |
Symbol.SPOT
Specifies spot weld symbol
|
static Symbol |
Symbol.SQUARE_BUTT
Specifies square butt weld symbol
|
static Symbol |
Symbol.STEEP_FLANKED_BEVEL
Specifies steeep flanked bevel butt weld symbol ( ISO and DIN only)
|
static Symbol |
Symbol.STEEP_FLANKED_V
Specifies steep flanked V butt weld symbol (ISO and DIN only)
|
static Symbol |
Symbol.STUD
Specifies stud weld symbol (Arrow side only )
|
static Symbol |
Symbol.SURFACE_JOINT
Specifies surface joint weld symbol (ISO and DIN only )
|
static Symbol |
Symbol.SURFACING
Specifies surfacing weld symbol (ISO and DIN only)
|
static Symbol |
Symbol.UBUTT
Specifies U butt weld symbol
|
static Symbol |
Symbol.VBUTT
Specifies V butt weld symbol
|
static Symbol |
Symbol.VBUTT_BROAD_ROOT_FACE
Specifies V butt with broad root face weld symbol (ISO and DIN only)
|
Modifier and Type | Method and Description |
---|---|
Symbol |
LineWeldSideData.symbol()
Returns the elementary weld symbol
License requirements: None. |
static Symbol |
Symbol.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Symbol |
Symbol.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Symbol[] |
Symbol.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LineWeldSideData.setSymbol(Symbol symbol)
Sets the elementary weld symbol
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
Symbol |
JointExitBuilder.otherSideSymbol()
Returns the symbol for welding other side when it is not being prepared
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
JointExitBuilder.setOtherSideSymbol(Symbol symbol)
License requirements: structure_weld ("STRUCTURE WELD") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.