Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static SurfaceFinishBuilder.StandardType |
SurfaceFinishBuilder.StandardType.ANSI
ANSI
|
static SurfaceFinishBuilder.StandardType |
SurfaceFinishBuilder.StandardType.DIN
DIN
|
static SurfaceFinishBuilder.StandardType |
SurfaceFinishBuilder.StandardType.DIN2002
DIN 2002
|
static SurfaceFinishBuilder.StandardType |
SurfaceFinishBuilder.StandardType.ESKD
ESKD
|
static SurfaceFinishBuilder.StandardType |
SurfaceFinishBuilder.StandardType.GB
GB131-93
|
static SurfaceFinishBuilder.StandardType |
SurfaceFinishBuilder.StandardType.ISO
ISO
|
static SurfaceFinishBuilder.StandardType |
SurfaceFinishBuilder.StandardType.ISO2002
ISO 2002
|
static SurfaceFinishBuilder.StandardType |
SurfaceFinishBuilder.StandardType.JIS
JIS
|
Modifier and Type | Method and Description |
---|---|
SurfaceFinishBuilder.StandardType |
SurfaceFinishBuilder.standard()
Returns the standard
License requirements: None. |
static SurfaceFinishBuilder.StandardType |
SurfaceFinishBuilder.StandardType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SurfaceFinishBuilder.StandardType |
SurfaceFinishBuilder.StandardType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SurfaceFinishBuilder.StandardType[] |
SurfaceFinishBuilder.StandardType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SurfaceFinishBuilder.setStandard(SurfaceFinishBuilder.StandardType standard)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.