Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
PmiAttributeValueInteger
Represents a PMI Attribute Integer Value
To create or edit an instance of this class, use PmiAttributeValueIntegerBuilder Created in NX6.0.0 |
interface |
PmiAttributeValueList
Represents a PMI Attribute List Value
To create or edit an instance of this class, use PmiAttributeValueListBuilder Created in NX6.0.0 |
interface |
PmiAttributeValueMultipleString
Represents a PMI Attribute MultipleString Value
To create or edit an instance of this class, use nxopen.annotations.PmiAttributeValueMultipleStringBuilder Created in NX6.0.0 |
interface |
PmiAttributeValueNumber
Represents a PMI Attribute Number Value
To create or edit an instance of this class, use PmiAttributeValueNumberBuilder Created in NX6.0.0 |
interface |
PmiAttributeValueString
Represents a PMI Attribute String Value
To create or edit an instance of this class, use nxopen.annotations.PmiAttributeValueStringBuilder Created in NX6.0.0 |
interface |
PmiAttributeValueUrl
Represents a PMI Attribute Url Value
To create or edit an instance of this class, use PmiAttributeValueUrlBuilder Created in NX6.0.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.