Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
OrdinateDoglegDefinition |
OrdinateDimension.DoglegPreferences.doglegSetting |
static OrdinateDoglegDefinition |
OrdinateDoglegDefinition.END_ANGLE
Specifies end offset and dogleg angle defined
|
static OrdinateDoglegDefinition |
OrdinateDoglegDefinition.LAST
Last enum value.
|
static OrdinateDoglegDefinition |
OrdinateDoglegDefinition.START_AND_END
Specifies start and end offeset defined
|
static OrdinateDoglegDefinition |
OrdinateDoglegDefinition.START_ANGLE
Specifies start offset and dogleg angle defined
|
Modifier and Type | Method and Description |
---|---|
OrdinateDoglegDefinition |
OrdinateDimensionPreferences.doglegDefinition()
Returns the dogleg definition
License requirements: None. |
OrdinateDoglegDefinition |
OrdinateStyleBuilder.doglegSetting()
Returns the dogleg setting.
|
static OrdinateDoglegDefinition |
OrdinateDoglegDefinition.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrdinateDoglegDefinition |
OrdinateDoglegDefinition.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrdinateDoglegDefinition[] |
OrdinateDoglegDefinition.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrdinateDimensionPreferences.setDoglegDefinition(OrdinateDoglegDefinition definition)
Sets the dogleg definition
License requirements: None. |
void |
OrdinateStyleBuilder.setDoglegSetting(OrdinateDoglegDefinition doglegSetting)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
Constructor and Description |
---|
DoglegPreferences(OrdinateDoglegDefinition doglegSettingInitial,
double angleInitial,
double startOffsetInitial,
double endOffsetInitial,
OrdinateDoglegCreationOption doglegOptionInitial)
Constructor for the DoglegPreferences object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.