Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Method and Description |
---|---|
MasterSymbolListItemBuilder |
CustomSymbolCollection.createMasterSymbolListItemBuilder()
Creates the Master Symbol List Item builder
License requirements: None. |
MasterSymbolListItemBuilder |
MasterSymbolBuilder.createNewListItem(Annotation noteTag,
String[] notes)
Create Master Symbol list item builder
License requirements: None. |
MasterSymbolListItemBuilder |
MasterSymbolListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
MasterSymbolListItemBuilder[] |
MasterSymbolListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
MasterSymbolListItemBuilderList.append(MasterSymbolListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
MasterSymbolListItemBuilderList.append(MasterSymbolListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
MasterSymbolListItemBuilderList.erase(MasterSymbolListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
MasterSymbolListItemBuilderList.erase(MasterSymbolListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
MasterSymbolListItemBuilderList.findIndex(MasterSymbolListItemBuilder obj)
Finds the index where the input object appears.
|
void |
MasterSymbolListItemBuilderList.insert(int location,
MasterSymbolListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
MasterSymbolListItemBuilderList.setContents(MasterSymbolListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
MasterSymbolListItemBuilderList.swap(MasterSymbolListItemBuilder object1,
MasterSymbolListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.