Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static JogOrientation |
JogOrientation.JOG_IN
Jog orientation in
|
static JogOrientation |
JogOrientation.JOG_OUT
Jog orientation out
|
Modifier and Type | Method and Description |
---|---|
JogOrientation |
LineArrowStyleBuilder.firstJogOrientation()
Returns the first jog orientation, can be either IN or OUT
License requirements: None. |
JogOrientation |
LineArrowStyleBuilder.secondJogOrientation()
Returns the second jog orientation, can be either IN or OUT
License requirements: None. |
static JogOrientation |
JogOrientation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static JogOrientation |
JogOrientation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static JogOrientation[] |
JogOrientation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LineArrowStyleBuilder.setFirstJogOrientation(JogOrientation jogOrientation)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
LineArrowStyleBuilder.setSecondJogOrientation(JogOrientation jogOrientation)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.