Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static HoleCalloutSettingsBuilder.Featuretype |
HoleCalloutSettingsBuilder.Featuretype.DRILL_SIZE_HOLE |
static HoleCalloutSettingsBuilder.Featuretype |
HoleCalloutSettingsBuilder.Featuretype.GENERAL_HOLE |
static HoleCalloutSettingsBuilder.Featuretype |
HoleCalloutSettingsBuilder.Featuretype.NONE |
static HoleCalloutSettingsBuilder.Featuretype |
HoleCalloutSettingsBuilder.Featuretype.SCREW_CLEARANCE_HOLE |
static HoleCalloutSettingsBuilder.Featuretype |
HoleCalloutSettingsBuilder.Featuretype.SYMBOLIC_THREAD |
static HoleCalloutSettingsBuilder.Featuretype |
HoleCalloutSettingsBuilder.Featuretype.THREADED_HOLE |
Modifier and Type | Method and Description |
---|---|
HoleCalloutSettingsBuilder.Featuretype[] |
HoleCalloutSettingsBuilder.getListOfFeatures()
Gets the list of features.
|
static HoleCalloutSettingsBuilder.Featuretype |
HoleCalloutSettingsBuilder.Featuretype.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HoleCalloutSettingsBuilder.Featuretype |
HoleCalloutSettingsBuilder.Featuretype.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HoleCalloutSettingsBuilder.Featuretype[] |
HoleCalloutSettingsBuilder.Featuretype.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HoleCalloutSettingsBuilder.deleteLineBreak(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth)
If the nth hole feature parameter of feature type is a line break and it can be deleted, deletes it.
|
HoleCalloutSettingsBuilder.Parametertype[] |
HoleCalloutSettingsBuilder.getListOfParameters(HoleCalloutSettingsBuilder.Featuretype featureType)
Gets the list of parameters for feature type.
|
boolean |
HoleCalloutSettingsBuilder.getNthParameterDisplay(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth)
Gets the display status of the nth hole feature parameter of feature type.
|
String[] |
HoleCalloutSettingsBuilder.getNthParameterPrefix(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth)
If the nth hole feature parameter of feature type can have prefix, gets its prefix.
|
StyleBuilder |
HoleCalloutSettingsBuilder.getNthParameterStyle(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth)
Gets the parameter style of the nth hole feature parameter of feature type.
|
String[] |
HoleCalloutSettingsBuilder.getNthParameterSuffix(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth)
If the nth hole feature parameter of feature type can have suffix, gets its suffix.
|
String |
HoleCalloutSettingsBuilder.getNthParameterValue(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth)
Gets the parameter expression of the nth hole feature parameter of feature type.
|
void |
HoleCalloutSettingsBuilder.insertLineBreak(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth)
If a line break can be inserted immediately after the nth hole feature parameter of feature type, inserts a line break at that position.
|
boolean |
HoleCalloutSettingsBuilder.reorderParameters(HoleCalloutSettingsBuilder.Featuretype featureType,
HoleCalloutSettingsBuilder.Parametertype[] parameters)
Reorder the parameters based on the input.
|
void |
HoleCalloutSettingsBuilder.setNthParameterDisplay(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth,
boolean parameterDisplay)
Sets the display status of the nth hole feature parameter of feature type.
|
void |
HoleCalloutSettingsBuilder.setNthParameterPrefix(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth,
String[] lines)
If the prefix of the nth hole feature parameter of feature type can be edited, sets its prefix.
|
void |
HoleCalloutSettingsBuilder.setNthParameterSuffix(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth,
String[] lines)
If the suffix of the nth hole feature parameter of feature type can be edited, sets its suffix.
|
void |
HoleCalloutSettingsBuilder.setNthParameterValue(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth,
String value)
Sets the parameter expression of the nth hole feature parameter of feature type.
|
void |
HoleCalloutSettingsBuilder.shiftDown(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth)
If the position of the nth hole feature parameter of feature type can be shifted down, shifts it down by one.
|
void |
HoleCalloutSettingsBuilder.shiftUp(HoleCalloutSettingsBuilder.Featuretype featureType,
int nth)
If the position of the nth hole feature parameter of feature type can be shifted up, shifts it up by one.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.