Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static FitAssemblyDisplayStyle |
FitAssemblyDisplayStyle.SINGLE_LINE
Display single line
|
static FitAssemblyDisplayStyle |
FitAssemblyDisplayStyle.TWO_LINES_ALIGNED
Display hole and shaft with dimension text aligned
|
static FitAssemblyDisplayStyle |
FitAssemblyDisplayStyle.TWO_LINES_CENTERED
Display hole and shaft with dimension text centered
|
Modifier and Type | Method and Description |
---|---|
FitAssemblyDisplayStyle |
DimensionStyleBuilder.limitFitAssemblyDisplayStyle()
Returns the dimension limit fit assembly display style.
|
FitAssemblyDisplayStyle |
DimensionPreferences.limitFitAssemblyDisplayStyle()
Returns the display style of fit tolerance for assembly dimensions.
|
static FitAssemblyDisplayStyle |
FitAssemblyDisplayStyle.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FitAssemblyDisplayStyle |
FitAssemblyDisplayStyle.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FitAssemblyDisplayStyle[] |
FitAssemblyDisplayStyle.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DimensionStyleBuilder.setLimitFitAssemblyDisplayStyle(FitAssemblyDisplayStyle fitAssemblyDisplayStyle)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
DimensionPreferences.setLimitFitAssemblyDisplayStyle(FitAssemblyDisplayStyle fitAssemblyDisplayStyle)
Sets the display style of fit tolerance for assembly dimensions.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.