Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Method and Description |
---|---|
FeatureControlFrameDataBuilder |
AnnotationManager.createFeatureControlFrameDataBuilder(FeatureControlFrameData frame)
Creates a
FeatureControlFrameDataBuilder
License requirements: None. |
FeatureControlFrameDataBuilder[] |
FeatureControlFrameBuilder.featureControlFrameData()
The feature control frame data list
License requirements: None. |
FeatureControlFrameDataBuilder |
FeatureControlFrameDataBuilderList.findItem(int index)
Returns the object at the input index.
|
FeatureControlFrameDataBuilder[] |
FeatureControlFrameDataBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
FeatureControlFrameDataBuilderList.append(FeatureControlFrameDataBuilder object)
Appends an object to the list
License requirements: None. |
void |
FeatureControlFrameDataBuilderList.append(FeatureControlFrameDataBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
FeatureControlFrameDataBuilderList.erase(FeatureControlFrameDataBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
FeatureControlFrameDataBuilderList.erase(FeatureControlFrameDataBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
FeatureControlFrameDataBuilderList.findIndex(FeatureControlFrameDataBuilder obj)
Finds the index where the input object appears.
|
void |
FeatureControlFrameDataBuilderList.insert(int location,
FeatureControlFrameDataBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
FeatureControlFrameDataBuilderList.setContents(FeatureControlFrameDataBuilder[] objects)
Sets the contents of the entire list.
|
void |
FeatureControlFrameDataBuilderList.swap(FeatureControlFrameDataBuilder object1,
FeatureControlFrameDataBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.