Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static DrivingValueBuilder.DrivingValueMethod |
DrivingValueBuilder.DrivingValueMethod.DRIVING |
static DrivingValueBuilder.DrivingValueMethod |
DrivingValueBuilder.DrivingValueMethod.INFERRED |
static DrivingValueBuilder.DrivingValueMethod |
DrivingValueBuilder.DrivingValueMethod.REFERENCE |
Modifier and Type | Method and Description |
---|---|
DrivingValueBuilder.DrivingValueMethod |
DrivingValueBuilder.drivingMethod()
Returns the driving method
License requirements: None. |
static DrivingValueBuilder.DrivingValueMethod |
DrivingValueBuilder.DrivingValueMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrivingValueBuilder.DrivingValueMethod |
DrivingValueBuilder.DrivingValueMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrivingValueBuilder.DrivingValueMethod[] |
DrivingValueBuilder.DrivingValueMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrivingValueBuilder.setDrivingMethod(DrivingValueBuilder.DrivingValueMethod drivingMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.