Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static DisplayPmiEffectivityMethod |
DisplayPmiEffectivityMethod.ALL_ASSOC_OCC_LOADED |
static DisplayPmiEffectivityMethod |
DisplayPmiEffectivityMethod.ANY_ASSOC_OCC_LOADED |
Modifier and Type | Method and Description |
---|---|
DisplayPmiEffectivityMethod |
PmiPreferences.displayPmiEffectivityMethod()
Returns the value indicating precise option of PMI Effectivity for prime geometry
License requirements: None. |
DisplayPmiEffectivityMethod |
PmiPreferences.displayPmiEffectivityReferenceMethod()
Returns the value indicating precise option of PMI Effectivity for reference geometry
License requirements: None. |
static DisplayPmiEffectivityMethod |
DisplayPmiEffectivityMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DisplayPmiEffectivityMethod |
DisplayPmiEffectivityMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DisplayPmiEffectivityMethod[] |
DisplayPmiEffectivityMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PmiPreferences.setDisplayPmiEffectivityMethod(DisplayPmiEffectivityMethod displayPmiEffectivityMethod)
License requirements: nx_pmi_effectivity ("NX PMI EFFECTIVITY") . |
void |
PmiPreferences.setDisplayPmiEffectivityReferenceMethod(DisplayPmiEffectivityMethod displayPmiEffectivityReferenceMethod)
License requirements: nx_pmi_effectivity ("NX PMI EFFECTIVITY") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.