Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static DatumTargetBuilder.StandardTypes |
DatumTargetBuilder.StandardTypes.ASIG2000
ASIG_2000
|
static DatumTargetBuilder.StandardTypes |
DatumTargetBuilder.StandardTypes.ASME_ISO11011983
ISO 1101 1983
|
static DatumTargetBuilder.StandardTypes |
DatumTargetBuilder.StandardTypes.ASME_Y1452009
ASME_Y145_2009
|
static DatumTargetBuilder.StandardTypes |
DatumTargetBuilder.StandardTypes.ASME_Y145M1982
ASME_Y145M_1982
|
static DatumTargetBuilder.StandardTypes |
DatumTargetBuilder.StandardTypes.ASME_Y145M1994
Y145M_1994
|
static DatumTargetBuilder.StandardTypes |
DatumTargetBuilder.StandardTypes.GM_ADDENDUM94
94_GM_ADDENDUM
|
static DatumTargetBuilder.StandardTypes |
DatumTargetBuilder.StandardTypes.NO_STANDARD
NO_STANDARD
|
Modifier and Type | Method and Description |
---|---|
DatumTargetBuilder.StandardTypes |
DatumTargetBuilder.datumTargetStandard()
Returns the datum target standard.
|
static DatumTargetBuilder.StandardTypes |
DatumTargetBuilder.StandardTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumTargetBuilder.StandardTypes |
DatumTargetBuilder.StandardTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumTargetBuilder.StandardTypes[] |
DatumTargetBuilder.StandardTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumTargetBuilder.setDatumTargetStandard(DatumTargetBuilder.StandardTypes standard)
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.