Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static CuttingPlaneSymbolBuilder.ViewNameFormatOption |
CuttingPlaneSymbolBuilder.ViewNameFormatOption.A
View Name is in the 'Section Prefix A' format, Where Section Prefix is taken from PMI Preferences
and A is the Text of the PMI Cutting Plane Symbol.
|
static CuttingPlaneSymbolBuilder.ViewNameFormatOption |
CuttingPlaneSymbolBuilder.ViewNameFormatOption.AA
View Name is in the 'Section Prefix A-A' format, Where Where Section Prefix is taken from PMI Preferences
and A is the Text of the PMI Cutting Plane Symbol.
|
static CuttingPlaneSymbolBuilder.ViewNameFormatOption |
CuttingPlaneSymbolBuilder.ViewNameFormatOption.USER_DEFINED
User Defined View Name
|
Modifier and Type | Method and Description |
---|---|
static CuttingPlaneSymbolBuilder.ViewNameFormatOption |
CuttingPlaneSymbolBuilder.ViewNameFormatOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CuttingPlaneSymbolBuilder.ViewNameFormatOption |
CuttingPlaneSymbolBuilder.ViewNameFormatOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CuttingPlaneSymbolBuilder.ViewNameFormatOption[] |
CuttingPlaneSymbolBuilder.ViewNameFormatOption.values()
Returns an array that contains the values for this enum.
|
CuttingPlaneSymbolBuilder.ViewNameFormatOption |
CuttingPlaneSymbolBuilder.viewNameFormat()
Returns the name view from symbol
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
CuttingPlaneSymbolBuilder.setViewNameFormat(CuttingPlaneSymbolBuilder.ViewNameFormatOption viewNameFormat)
License requirements: geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.