Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static Constants |
Constants.MAX_LEADER_INTERMEDIATE_POINTS
The maximum number of intermediate points that a leader can have
|
static Constants |
Constants.MAX_LEADERS
The maximum number of leaders that an annotation can have
|
Modifier and Type | Method and Description |
---|---|
static Constants |
Constants.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Constants |
Constants.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Constants[] |
Constants.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.