Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
BaseCenterline3d
Represents a Base 3D centerline
This is an abstract class. |
interface |
BaseCenterMark
Represents a base center mark class
This is an abstract class. |
interface |
BoltCircleCenterline
Represents a BoltCircleCenterline centerline
To create or edit an instance of this class, use BoltCircleCenterlineBuilder Created in NX6.0.0 |
interface |
Centerline2d
Represents a 2D centerline
To create or edit an instance of this class, use Centerline2dBuilder Created in NX6.0.0 |
interface |
Centerline3d
Represents a 3D centerline
To create or edit an instance of this class, use Centerline3dBuilder Created in NX6.0.0 |
interface |
CenterMark
Represents a center mark class
To create or edit an instance of this class, use CenterMarkBuilder Created in NX6.0.0 |
interface |
CircleCenterline
Represents a CircleCenterline centerline
This is an abstract class. |
interface |
CircularCenterline
Represents a CircularCenterline centerline
To create or edit an instance of this class, use CircularCenterlineBuilder Created in NX6.0.0 |
interface |
PmiCenterline3d
Represents a Pmi 3D centerline
To create or edit an instance of this class, use PmiCenterline3dBuilder Created in NX7.5.0 |
interface |
PmiCenterMark
Represents a PMI Center Mark class
To create or edit an instance of this class, use PmiCenterMarkBuilder Created in NX7.5.0 |
interface |
SymmetricalCenterline
Represents a Symmetrical Centerline
To create or edit an instance of this class, use SymmetricalCenterlineBuilder Created in NX6.0.0 |
Modifier and Type | Method and Description |
---|---|
Centerline |
CenterlineCollection.findObject(String journalIdentifier)
Finds the Centerline with the given name.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.