Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static BillOfMaterialBuilder.StockLengthType |
BillOfMaterialBuilder.StockLengthType.LIST_EACH |
static BillOfMaterialBuilder.StockLengthType |
BillOfMaterialBuilder.StockLengthType.SINGLE_SUM |
Modifier and Type | Method and Description |
---|---|
BillOfMaterialBuilder.StockLengthType |
BillOfMaterialBuilder.stockLength()
Returns the value that specifies the stock length type.
|
static BillOfMaterialBuilder.StockLengthType |
BillOfMaterialBuilder.StockLengthType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BillOfMaterialBuilder.StockLengthType |
BillOfMaterialBuilder.StockLengthType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BillOfMaterialBuilder.StockLengthType[] |
BillOfMaterialBuilder.StockLengthType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BillOfMaterialBuilder.setStockLength(BillOfMaterialBuilder.StockLengthType stockLength)
License requirements: routing_base ("Routing Basic") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.