public interface SymbolCatalogBuilder extends Builder
CustomSymbolCollection.createSymbolCatalogBuilder()
Modifier and Type | Method and Description |
---|---|
void |
generateItemNumber()
Deprecated.
Deprecated in NX10.0.0. Use
JA_SYMBOL_CATALOG_BUILDER_set_ItemNumber instead.
|
void |
generateRevision()
Deprecated.
Deprecated in NX10.0.0. Use
JA_SYMBOL_CATALOG_BUILDER_set_Revision instead.
|
PartOperationCreateBuilder |
getPartOperationCreateBuilder()
Gets
PartOperationBuilder
License requirements: None. |
boolean |
isPartSymbol()
Returns the variable of is part symbol or not, get it from the reuse library
License requirements: None. |
String |
itemName()
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCreateBuilder instead.
|
String |
itemNumber()
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCreateBuilder instead.
|
SymbolCatalogParameterBuilder |
newParameter()
Creates a
SymbolCatalogParameterBuilder object. |
String |
nodeString()
Returns the node string of the fastener symbol,
NOTE: Client must free the returned TEXT_p_t* with TEXT_free
License requirements: None. |
SymbolCatalogParameterBuilderList |
parameterList()
Returns the list containing the parameters used to create the symbol.
|
String |
partFileName()
Returns the part file name,
NOTE: Client must free the returned TEXT_p_t* with TEXT_free
License requirements: None. |
String |
path()
Returns the path, get it from the reuse library
NOTE: Client must free the returned TEXT_p_t* with TEXT_free
License requirements: None. |
String |
revision()
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCreateBuilder instead.
|
void |
setItemName(String itemName)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCreateBuilder instead.
|
void |
setItemNumber(String itemNumber)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCreateBuilder instead.
|
void |
setNodeString(String nodeString)
License requirements: nx_layout ("NX Layout") . |
void |
setPartFileName(String partFileName)
License requirements: nx_layout ("NX Layout") . |
void |
setPartOperationCreateBuilder(PartOperationCreateBuilder partOperationBuilder)
|
void |
setPartSymbol(boolean isPartSymbol)
License requirements: nx_layout ("NX Layout") . |
void |
setPath(String path)
License requirements: nx_layout ("NX Layout") . |
void |
setRevision(String revision)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCreateBuilder instead.
|
void |
setSymbolName(String symbolName)
License requirements: nx_layout ("NX Layout") . |
String |
symbolName()
Returns the JA method support for accessing and setting Symbol Name value,
NOTE: Client must free the returned TEXT_p_t* with TEXT_free
License requirements: None. |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
String nodeString() throws NXException, RemoteException
NXException
RemoteException
void setNodeString(String nodeString) throws NXException, RemoteException
nodeString
- NXException
RemoteException
SymbolCatalogParameterBuilderList parameterList() throws NXException, RemoteException
NXException
RemoteException
String symbolName() throws NXException, RemoteException
NXException
RemoteException
void setSymbolName(String symbolName) throws NXException, RemoteException
symbolName
- NXException
RemoteException
String partFileName() throws NXException, RemoteException
NXException
RemoteException
void setPartFileName(String partFileName) throws NXException, RemoteException
partFileName
- NXException
RemoteException
String itemNumber() throws NXException, RemoteException
PartOperationCreateBuilder
instead.
NXException
RemoteException
void setItemNumber(String itemNumber) throws NXException, RemoteException
PartOperationCreateBuilder
instead.
itemNumber
- NXException
RemoteException
String revision() throws NXException, RemoteException
PartOperationCreateBuilder
instead.
NXException
RemoteException
void setRevision(String revision) throws NXException, RemoteException
PartOperationCreateBuilder
instead.
revision
- NXException
RemoteException
String itemName() throws NXException, RemoteException
PartOperationCreateBuilder
instead.
NXException
RemoteException
void setItemName(String itemName) throws NXException, RemoteException
PartOperationCreateBuilder
instead.
itemName
- NXException
RemoteException
void generateItemNumber() throws NXException, RemoteException
JA_SYMBOL_CATALOG_BUILDER_set_ItemNumber
instead.
NXException
RemoteException
void generateRevision() throws NXException, RemoteException
JA_SYMBOL_CATALOG_BUILDER_set_Revision
instead.
NXException
RemoteException
String path() throws NXException, RemoteException
NXException
RemoteException
void setPath(String path) throws NXException, RemoteException
path
- location of symbolNXException
RemoteException
boolean isPartSymbol() throws NXException, RemoteException
NXException
RemoteException
void setPartSymbol(boolean isPartSymbol) throws NXException, RemoteException
isPartSymbol
- True If it is part symbolNXException
RemoteException
SymbolCatalogParameterBuilder newParameter() throws NXException, RemoteException
SymbolCatalogParameterBuilder
object.
NXException
RemoteException
void setPartOperationCreateBuilder(PartOperationCreateBuilder partOperationBuilder) throws NXException, RemoteException
partOperationBuilder
- NXException
RemoteException
PartOperationCreateBuilder getPartOperationCreateBuilder() throws NXException, RemoteException
NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.