public static class LineWeldDataBuilder.ContourSymbolType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BACKING_STRIP_PERMANENT_ISO_AND_DIN_ONLY |
static int |
_BACKING_STRIP_REMOVABLE_ISO_AND_DIN_ONLY |
static int |
_BLENDED_TOES_ISO_AND_DIN_ONLY |
static int |
_CONCAVE |
static int |
_CONVEX |
static int |
_FLAT |
static int |
_FLUSH |
static int |
_MACHINING_GRADED_JUNCTION |
static int |
_NONE |
static LineWeldDataBuilder.ContourSymbolType |
BACKING_STRIP_PERMANENT_ISO_AND_DIN_ONLY |
static LineWeldDataBuilder.ContourSymbolType |
BACKING_STRIP_REMOVABLE_ISO_AND_DIN_ONLY |
static LineWeldDataBuilder.ContourSymbolType |
BLENDED_TOES_ISO_AND_DIN_ONLY |
static LineWeldDataBuilder.ContourSymbolType |
CONCAVE |
static LineWeldDataBuilder.ContourSymbolType |
CONVEX |
static LineWeldDataBuilder.ContourSymbolType |
FLAT |
static LineWeldDataBuilder.ContourSymbolType |
FLUSH |
static LineWeldDataBuilder.ContourSymbolType |
MACHINING_GRADED_JUNCTION |
static LineWeldDataBuilder.ContourSymbolType |
NONE |
Modifier and Type | Method and Description |
---|---|
static LineWeldDataBuilder.ContourSymbolType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LineWeldDataBuilder.ContourSymbolType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LineWeldDataBuilder.ContourSymbolType[] |
values()
Returns an array that contains the values for this enum.
|
public static final LineWeldDataBuilder.ContourSymbolType NONE
public static final LineWeldDataBuilder.ContourSymbolType CONVEX
public static final LineWeldDataBuilder.ContourSymbolType FLAT
public static final LineWeldDataBuilder.ContourSymbolType CONCAVE
public static final LineWeldDataBuilder.ContourSymbolType BLENDED_TOES_ISO_AND_DIN_ONLY
public static final LineWeldDataBuilder.ContourSymbolType BACKING_STRIP_PERMANENT_ISO_AND_DIN_ONLY
public static final LineWeldDataBuilder.ContourSymbolType BACKING_STRIP_REMOVABLE_ISO_AND_DIN_ONLY
public static final LineWeldDataBuilder.ContourSymbolType FLUSH
public static final LineWeldDataBuilder.ContourSymbolType MACHINING_GRADED_JUNCTION
public static final int _NONE
public static final int _CONVEX
public static final int _FLAT
public static final int _CONCAVE
public static final int _BLENDED_TOES_ISO_AND_DIN_ONLY
public static final int _BACKING_STRIP_PERMANENT_ISO_AND_DIN_ONLY
public static final int _BACKING_STRIP_REMOVABLE_ISO_AND_DIN_ONLY
public static final int _FLUSH
public static final int _MACHINING_GRADED_JUNCTION
public static LineWeldDataBuilder.ContourSymbolType valueOf(int value)
public static LineWeldDataBuilder.ContourSymbolType valueOf(String name)
public static LineWeldDataBuilder.ContourSymbolType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.