public static class HoleTableSettingsHoleFiltersBuilder.ScopeType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ONE_SIDED_HOLES
One-sided Holes
|
static int |
_TWO_SIDED_HOLES
Two-sided Holes
|
static HoleTableSettingsHoleFiltersBuilder.ScopeType |
ONE_SIDED_HOLES
One-sided Holes
|
static HoleTableSettingsHoleFiltersBuilder.ScopeType |
TWO_SIDED_HOLES
Two-sided Holes
|
Modifier and Type | Method and Description |
---|---|
static HoleTableSettingsHoleFiltersBuilder.ScopeType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HoleTableSettingsHoleFiltersBuilder.ScopeType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HoleTableSettingsHoleFiltersBuilder.ScopeType[] |
values()
Returns an array that contains the values for this enum.
|
public static final HoleTableSettingsHoleFiltersBuilder.ScopeType ONE_SIDED_HOLES
public static final HoleTableSettingsHoleFiltersBuilder.ScopeType TWO_SIDED_HOLES
public static final int _ONE_SIDED_HOLES
public static final int _TWO_SIDED_HOLES
public static HoleTableSettingsHoleFiltersBuilder.ScopeType valueOf(int value)
public static HoleTableSettingsHoleFiltersBuilder.ScopeType valueOf(String name)
public static HoleTableSettingsHoleFiltersBuilder.ScopeType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.