public class FitAssemblyDisplayStyle extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SINGLE_LINE
Display single line
|
static int |
_TWO_LINES_ALIGNED
Display hole and shaft with dimension text aligned
|
static int |
_TWO_LINES_CENTERED
Display hole and shaft with dimension text centered
|
static FitAssemblyDisplayStyle |
SINGLE_LINE
Display single line
|
static FitAssemblyDisplayStyle |
TWO_LINES_ALIGNED
Display hole and shaft with dimension text aligned
|
static FitAssemblyDisplayStyle |
TWO_LINES_CENTERED
Display hole and shaft with dimension text centered
|
Modifier and Type | Method and Description |
---|---|
static FitAssemblyDisplayStyle |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FitAssemblyDisplayStyle |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FitAssemblyDisplayStyle[] |
values()
Returns an array that contains the values for this enum.
|
public static final FitAssemblyDisplayStyle SINGLE_LINE
public static final FitAssemblyDisplayStyle TWO_LINES_CENTERED
public static final FitAssemblyDisplayStyle TWO_LINES_ALIGNED
public static final int _SINGLE_LINE
public static final int _TWO_LINES_CENTERED
public static final int _TWO_LINES_ALIGNED
public static FitAssemblyDisplayStyle valueOf(int value)
public static FitAssemblyDisplayStyle valueOf(String name)
public static FitAssemblyDisplayStyle[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.