public class ExtensionLineDisplay extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FIRST
Displays extension line attached to the
first object selected to create the dimension
|
static int |
_LAST
Last enum value.
|
static int |
_NONE
Doesn't display extension lines
|
static int |
_SECOND
Displays extension line attached to the
second object selected to create the dimension
|
static int |
_TWO
Displays both the extension lines
|
static ExtensionLineDisplay |
FIRST
Displays extension line attached to the
first object selected to create the dimension
|
static ExtensionLineDisplay |
LAST
Last enum value.
|
static ExtensionLineDisplay |
NONE
Doesn't display extension lines
|
static ExtensionLineDisplay |
SECOND
Displays extension line attached to the
second object selected to create the dimension
|
static ExtensionLineDisplay |
TWO
Displays both the extension lines
|
Modifier and Type | Method and Description |
---|---|
static ExtensionLineDisplay |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtensionLineDisplay |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtensionLineDisplay[] |
values()
Returns an array that contains the values for this enum.
|
public static final ExtensionLineDisplay TWO
public static final ExtensionLineDisplay FIRST
public static final ExtensionLineDisplay SECOND
public static final ExtensionLineDisplay NONE
public static final ExtensionLineDisplay LAST
public static final int _TWO
public static final int _FIRST
public static final int _SECOND
public static final int _NONE
public static final int _LAST
public static ExtensionLineDisplay valueOf(int value)
public static ExtensionLineDisplay valueOf(String name)
public static ExtensionLineDisplay[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.