public interface BaseNote extends NoteBase, IPmi
SimpleDraftingAid.UserSymbolSizeData
Modifier and Type | Method and Description |
---|---|
boolean |
isVertical()
Returns a flag indicating whether the note is vertical.
|
void |
setVertical(boolean isVertical)
Sets a flag indicating whether the note is vertical.
|
void |
updateFromRule()
Updates the specified note from the KF rule.
|
getText, getUserSymbolPreferences, getUserSymbolSize, setText, setUserSymbolPreferences, setUserSymbolSize
getAssociatedObject, getBusinessModifiers, getSharedAssociatedObject, index, isMirrored, setAssociatedObject, setBusinessModifiers, setIndex
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
void setVertical(boolean isVertical) throws NXException, RemoteException
Update.doUpdate(int)
.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object.
If it is, the changes will be overridden when the part is updated.
isVertical
- NXException
RemoteException
boolean isVertical() throws NXException, RemoteException
Update.doUpdate(int)
.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object.
If it is, the changes will be overridden when the part is updated.
NXException
RemoteException
void updateFromRule() throws NXException, RemoteException
Update.doUpdate(int)
.
NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.