public static class Validation.InputType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_APPLICATION
Input rules are from validation applications
|
static int |
_KF_CLASS
Input rules are in a KF class
|
static int |
_NUM
Last item define the number of the input source, not used as a type.
|
static int |
_SPREADSHEET
Input rules are from a spreadsheet
|
static int |
_TCR
Input rules are from TcR
|
static int |
_TEXT_FILE
Input rules are from a text file
|
static int |
_XML
Input rules are from XML file
|
static Validation.InputType |
APPLICATION
Input rules are from validation applications
|
static Validation.InputType |
KF_CLASS
Input rules are in a KF class
|
static Validation.InputType |
NUM
Last item define the number of the input source, not used as a type.
|
static Validation.InputType |
SPREADSHEET
Input rules are from a spreadsheet
|
static Validation.InputType |
TCR
Input rules are from TcR
|
static Validation.InputType |
TEXT_FILE
Input rules are from a text file
|
static Validation.InputType |
XML
Input rules are from XML file
|
Modifier and Type | Method and Description |
---|---|
static Validation.InputType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Validation.InputType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Validation.InputType[] |
values()
Returns an array that contains the values for this enum.
|
public static final Validation.InputType KF_CLASS
public static final Validation.InputType SPREADSHEET
public static final Validation.InputType TEXT_FILE
public static final Validation.InputType XML
public static final Validation.InputType TCR
public static final Validation.InputType APPLICATION
public static final Validation.InputType NUM
public static final int _KF_CLASS
public static final int _SPREADSHEET
public static final int _TEXT_FILE
public static final int _XML
public static final int _TCR
public static final int _APPLICATION
public static final int _NUM
public static Validation.InputType valueOf(int value)
public static Validation.InputType valueOf(String name)
public static Validation.InputType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.