public static class SketchPattern.InstanceControl extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FULL_CIRCLE
The pattern instance control type is Full Circle
|
static int |
_NUMBER_OFFSET
The pattern instance control type is number + offset
|
static SketchPattern.InstanceControl |
FULL_CIRCLE
The pattern instance control type is Full Circle
|
static SketchPattern.InstanceControl |
NUMBER_OFFSET
The pattern instance control type is number + offset
|
Modifier and Type | Method and Description |
---|---|
static SketchPattern.InstanceControl |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchPattern.InstanceControl |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchPattern.InstanceControl[] |
values()
Returns an array that contains the values for this enum.
|
public static final SketchPattern.InstanceControl FULL_CIRCLE
public static final SketchPattern.InstanceControl NUMBER_OFFSET
public static final int _FULL_CIRCLE
public static final int _NUMBER_OFFSET
public static SketchPattern.InstanceControl valueOf(int value)
public static SketchPattern.InstanceControl valueOf(String name)
public static SketchPattern.InstanceControl[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.