public interface SketchPasteBuilder extends Builder
SketchPasteBuilder
SketchCollection.createSketchPasteBuilder(nxopen.Sketch[])
Property | Value |
---|---|
MoveObject.Associative | false |
MoveObject.CreateTraceLines | false |
MoveObject.Divisions | 1 |
MoveObject.LayerOption | Original |
MoveObject.MoveObjectResult | MoveOriginal |
MoveObject.MoveParents | true |
MoveObject.NumberOfCopies | 1 |
MoveObject.TransformMotion.DeltaEnum | ReferenceWcsWorkPart |
MoveObject.TransformMotion.DeltaXc.Value | 0.0 |
MoveObject.TransformMotion.DeltaYc.Value | 0.0 |
MoveObject.TransformMotion.DeltaZc.Value | 0.0 |
MoveObject.TransformMotion.Option | Dynamic |
Modifier and Type | Method and Description |
---|---|
Point3d |
initialPasteLocation()
Returns the initial paste location, this is mainly used to define default paste location of sketch objects
License requirements: None. |
MoveObjectBuilder |
moveObject()
Returns the move object
License requirements: None. |
void |
resetInitialPasteLocation()
Reset the initial paste location, after this previously set initial paste location will not be used
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
void |
setInitialPasteLocation(Point3d dropLocation)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
MoveObjectBuilder moveObject() throws NXException, RemoteException
NXException
RemoteException
Point3d initialPasteLocation() throws NXException, RemoteException
NXException
RemoteException
void setInitialPasteLocation(Point3d dropLocation) throws NXException, RemoteException
dropLocation
- Drop location coordinates in absoluteNXException
RemoteException
void resetInitialPasteLocation() throws NXException, RemoteException
NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.