public static class Sketch.UpdateLevel extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MODEL
Update the full model and the sketch
|
static int |
_SKETCH_ONLY
Only update the sketch
|
static Sketch.UpdateLevel |
MODEL
Update the full model and the sketch
|
static Sketch.UpdateLevel |
SKETCH_ONLY
Only update the sketch
|
Modifier and Type | Method and Description |
---|---|
static Sketch.UpdateLevel |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.UpdateLevel |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.UpdateLevel[] |
values()
Returns an array that contains the values for this enum.
|
public static final Sketch.UpdateLevel SKETCH_ONLY
public static final Sketch.UpdateLevel MODEL
public static final int _SKETCH_ONLY
public static final int _MODEL
public static Sketch.UpdateLevel valueOf(int value)
public static Sketch.UpdateLevel valueOf(String name)
public static Sketch.UpdateLevel[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.