public static class Sketch.TrimInputOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FALSE
Do not trim the input curves
|
static int |
_TRUE
Trim the input curves
|
static Sketch.TrimInputOption |
FALSE
Do not trim the input curves
|
static Sketch.TrimInputOption |
TRUE
Trim the input curves
|
Modifier and Type | Method and Description |
---|---|
static Sketch.TrimInputOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.TrimInputOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.TrimInputOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final Sketch.TrimInputOption FALSE
public static final Sketch.TrimInputOption TRUE
public static final int _FALSE
public static final int _TRUE
public static Sketch.TrimInputOption valueOf(int value)
public static Sketch.TrimInputOption valueOf(String name)
public static Sketch.TrimInputOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.