public static class Sketch.Status extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INCONSISTENTLY_CONSTRAINED
The sketch has conflicting constraints
|
static int |
_NOT_EVALUATED |
static int |
_OVER_CONSTRAINED
The sketch has more constraints than is needed
|
static int |
_UNDER_CONSTRAINED
More constraints are needed to fully constrain the sketch
|
static int |
_UNKNOWN |
static int |
_WELL_CONSTRAINED
The sketch is fully constrained
|
static Sketch.Status |
INCONSISTENTLY_CONSTRAINED
The sketch has conflicting constraints
|
static Sketch.Status |
NOT_EVALUATED |
static Sketch.Status |
OVER_CONSTRAINED
The sketch has more constraints than is needed
|
static Sketch.Status |
UNDER_CONSTRAINED
More constraints are needed to fully constrain the sketch
|
static Sketch.Status |
UNKNOWN |
static Sketch.Status |
WELL_CONSTRAINED
The sketch is fully constrained
|
Modifier and Type | Method and Description |
---|---|
static Sketch.Status |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.Status |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.Status[] |
values()
Returns an array that contains the values for this enum.
|
public static final Sketch.Status UNKNOWN
public static final Sketch.Status NOT_EVALUATED
public static final Sketch.Status UNDER_CONSTRAINED
public static final Sketch.Status WELL_CONSTRAINED
public static final Sketch.Status OVER_CONSTRAINED
public static final Sketch.Status INCONSISTENTLY_CONSTRAINED
public static final int _UNKNOWN
public static final int _NOT_EVALUATED
public static final int _UNDER_CONSTRAINED
public static final int _WELL_CONSTRAINED
public static final int _OVER_CONSTRAINED
public static final int _INCONSISTENTLY_CONSTRAINED
public static Sketch.Status valueOf(int value)
public static Sketch.Status valueOf(String name)
public static Sketch.Status[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.