public static class ModelingViewHighQualityImage.FormatType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_QTVR_OBJECT_HIGH
Quick Time Virtual Reality object movie , which is a set of image of an
object in different rotations.
|
static int |
_QTVR_OBJECT_LOW
Quick Time Virtual Reality object movie, which is a set of image of an
object in different rotations.
|
static int |
_QTVR_PANORAMA
Quick Time Virtual Reality panoramic movie, which is a set of images
from a fixed viewpoint.
|
static int |
_RASTER_IMAGE
A normal single raster image
|
static ModelingViewHighQualityImage.FormatType |
QTVR_OBJECT_HIGH
Quick Time Virtual Reality object movie , which is a set of image of an
object in different rotations.
|
static ModelingViewHighQualityImage.FormatType |
QTVR_OBJECT_LOW
Quick Time Virtual Reality object movie, which is a set of image of an
object in different rotations.
|
static ModelingViewHighQualityImage.FormatType |
QTVR_PANORAMA
Quick Time Virtual Reality panoramic movie, which is a set of images
from a fixed viewpoint.
|
static ModelingViewHighQualityImage.FormatType |
RASTER_IMAGE
A normal single raster image
|
Modifier and Type | Method and Description |
---|---|
static ModelingViewHighQualityImage.FormatType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ModelingViewHighQualityImage.FormatType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ModelingViewHighQualityImage.FormatType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ModelingViewHighQualityImage.FormatType RASTER_IMAGE
public static final ModelingViewHighQualityImage.FormatType QTVR_PANORAMA
public static final ModelingViewHighQualityImage.FormatType QTVR_OBJECT_LOW
public static final ModelingViewHighQualityImage.FormatType QTVR_OBJECT_HIGH
public static final int _RASTER_IMAGE
public static final int _QTVR_PANORAMA
public static final int _QTVR_OBJECT_LOW
public static final int _QTVR_OBJECT_HIGH
public static ModelingViewHighQualityImage.FormatType valueOf(int value)
public static ModelingViewHighQualityImage.FormatType valueOf(String name)
public static ModelingViewHighQualityImage.FormatType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.