public static class MeasureDistanceBuilder.MeasureType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LOCAL_MINIMUM |
static int |
_MAX_CLEARANCE |
static int |
_MAXIMUM |
static int |
_MIN_CLEARANCE |
static int |
_MINIMUM |
static int |
_TO_APOINT |
static MeasureDistanceBuilder.MeasureType |
LOCAL_MINIMUM |
static MeasureDistanceBuilder.MeasureType |
MAX_CLEARANCE |
static MeasureDistanceBuilder.MeasureType |
MAXIMUM |
static MeasureDistanceBuilder.MeasureType |
MIN_CLEARANCE |
static MeasureDistanceBuilder.MeasureType |
MINIMUM |
static MeasureDistanceBuilder.MeasureType |
TO_APOINT |
Modifier and Type | Method and Description |
---|---|
static MeasureDistanceBuilder.MeasureType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeasureDistanceBuilder.MeasureType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeasureDistanceBuilder.MeasureType[] |
values()
Returns an array that contains the values for this enum.
|
public static final MeasureDistanceBuilder.MeasureType TO_APOINT
public static final MeasureDistanceBuilder.MeasureType MINIMUM
public static final MeasureDistanceBuilder.MeasureType LOCAL_MINIMUM
public static final MeasureDistanceBuilder.MeasureType MAXIMUM
public static final MeasureDistanceBuilder.MeasureType MIN_CLEARANCE
public static final MeasureDistanceBuilder.MeasureType MAX_CLEARANCE
public static final int _TO_APOINT
public static final int _MINIMUM
public static final int _LOCAL_MINIMUM
public static final int _MAXIMUM
public static final int _MIN_CLEARANCE
public static final int _MAX_CLEARANCE
public static MeasureDistanceBuilder.MeasureType valueOf(int value)
public static MeasureDistanceBuilder.MeasureType valueOf(String name)
public static MeasureDistanceBuilder.MeasureType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.