public static class LoadOptions.BookmarkComponents extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LOAD_LOADED
Load and show only what was loaded on the bookmark's save
Load invisible components and keep them invisible.
|
static int |
_LOAD_LOADED_AND_NON_DISPLAYED
Load and show only what was loaded on the bookmark's save, including non-display parts.
|
static int |
_LOAD_VISIBLE
Load and show only what was shown on the bookmark's save.
|
static int |
_NO_CHANGE
This option has no effect.
|
static LoadOptions.BookmarkComponents |
LOAD_LOADED
Load and show only what was loaded on the bookmark's save
Load invisible components and keep them invisible.
|
static LoadOptions.BookmarkComponents |
LOAD_LOADED_AND_NON_DISPLAYED
Load and show only what was loaded on the bookmark's save, including non-display parts.
|
static LoadOptions.BookmarkComponents |
LOAD_VISIBLE
Load and show only what was shown on the bookmark's save.
|
static LoadOptions.BookmarkComponents |
NO_CHANGE
This option has no effect.
|
Modifier and Type | Method and Description |
---|---|
static LoadOptions.BookmarkComponents |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LoadOptions.BookmarkComponents |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LoadOptions.BookmarkComponents[] |
values()
Returns an array that contains the values for this enum.
|
public static final LoadOptions.BookmarkComponents NO_CHANGE
public static final LoadOptions.BookmarkComponents LOAD_VISIBLE
public static final LoadOptions.BookmarkComponents LOAD_LOADED
public static final LoadOptions.BookmarkComponents LOAD_LOADED_AND_NON_DISPLAYED
public static final int _NO_CHANGE
public static final int _LOAD_VISIBLE
public static final int _LOAD_LOADED
public static final int _LOAD_LOADED_AND_NON_DISPLAYED
public static LoadOptions.BookmarkComponents valueOf(int value)
public static LoadOptions.BookmarkComponents valueOf(String name)
public static LoadOptions.BookmarkComponents[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.