public static class ListingWindow.DeviceType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FILE
Output is written to a file instead of the Information window
|
static int |
_FILE_AND_WINDOW
Output is written to a file and to the Information window
|
static int |
_NONE
Output is not written anywhere; output gets discarded
|
static int |
_WINDOW
The UI's Information window
|
static ListingWindow.DeviceType |
FILE
Output is written to a file instead of the Information window
|
static ListingWindow.DeviceType |
FILE_AND_WINDOW
Output is written to a file and to the Information window
|
static ListingWindow.DeviceType |
NONE
Output is not written anywhere; output gets discarded
|
static ListingWindow.DeviceType |
WINDOW
The UI's Information window
|
Modifier and Type | Method and Description |
---|---|
static ListingWindow.DeviceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ListingWindow.DeviceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ListingWindow.DeviceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ListingWindow.DeviceType WINDOW
public static final ListingWindow.DeviceType FILE
public static final ListingWindow.DeviceType FILE_AND_WINDOW
public static final ListingWindow.DeviceType NONE
public static final int _WINDOW
public static final int _FILE
public static final int _FILE_AND_WINDOW
public static final int _NONE
public static ListingWindow.DeviceType valueOf(int value)
public static ListingWindow.DeviceType valueOf(String name)
public static ListingWindow.DeviceType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.