public interface HumanReachZone extends TaggedObject
Modifier and Type | Interface and Description |
---|---|
static class |
HumanReachZone.Data
This class holds the data returned from
getData() |
static class |
HumanReachZone.MethodType
This enum represents the methods for computing the reach zone
|
Modifier and Type | Method and Description |
---|---|
void |
changeName(String reachZoneName)
Change reach zone name
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
NXObject |
geom()
Returns the geometry of reach zone
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
HumanReachZone.Data |
getData()
Get reach zone data
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
void |
setData(String zoneName,
HumanReachZone.MethodType method,
double waistFlexAngleData,
double waistFlexRangeLowerData,
double waistFlexRangeUpperData,
double waistLateralAngleData,
double waistLateralRangeLowerData,
double waistLateralRangeUpperData,
String traceSiteName,
Human human,
int resolution,
boolean assocReachZone)
Set reach zone data
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
printTestData, printTestData, tag, tagValue
void setData(String zoneName, HumanReachZone.MethodType method, double waistFlexAngleData, double waistFlexRangeLowerData, double waistFlexRangeUpperData, double waistLateralAngleData, double waistLateralRangeLowerData, double waistLateralRangeUpperData, String traceSiteName, Human human, int resolution, boolean assocReachZone) throws NXException, RemoteException
zoneName
- Name of the reach zone method
- Method used to create the reach zonewaistFlexAngleData
- Waist flex angle valuewaistFlexRangeLowerData
- Lower limit of waist flex anglewaistFlexRangeUpperData
- Upper limit of waist flex anglewaistLateralAngleData
- Waist lateral angle valuewaistLateralRangeLowerData
- Lower limit of waist lateral angle rangewaistLateralRangeUpperData
- upper limit of waist lateral angle rangetraceSiteName
- Name of the site traced to create the trace site human
- Human Featureresolution
- Resolution of the reach zoneassocReachZone
- Flag for associative reach zoneNXException
RemoteException
HumanReachZone.Data getData() throws NXException, RemoteException
NXException
RemoteException
void changeName(String reachZoneName) throws NXException, RemoteException
reachZoneName
- New name of the reach zone NXException
RemoteException
NXObject geom() throws NXException, RemoteException
NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.