public static class DisplayManager.LayerSetting extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CHANGE_LAYER_TO_SELECTABLE
Change the layer to selectable if it is invisible
|
static int |
_INVALID
Last value, should not be used.
|
static int |
_MOVE_OBJECTS_TO_WORK_LAYER
Move the objects to work layer if they are in invisible layer
|
static DisplayManager.LayerSetting |
CHANGE_LAYER_TO_SELECTABLE
Change the layer to selectable if it is invisible
|
static DisplayManager.LayerSetting |
INVALID
Last value, should not be used.
|
static DisplayManager.LayerSetting |
MOVE_OBJECTS_TO_WORK_LAYER
Move the objects to work layer if they are in invisible layer
|
Modifier and Type | Method and Description |
---|---|
static DisplayManager.LayerSetting |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DisplayManager.LayerSetting |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DisplayManager.LayerSetting[] |
values()
Returns an array that contains the values for this enum.
|
public static final DisplayManager.LayerSetting MOVE_OBJECTS_TO_WORK_LAYER
public static final DisplayManager.LayerSetting CHANGE_LAYER_TO_SELECTABLE
public static final DisplayManager.LayerSetting INVALID
public static final int _MOVE_OBJECTS_TO_WORK_LAYER
public static final int _CHANGE_LAYER_TO_SELECTABLE
public static final int _INVALID
public static DisplayManager.LayerSetting valueOf(int value)
public static DisplayManager.LayerSetting valueOf(String name)
public static DisplayManager.LayerSetting[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.