NXOpen.UF.Modeling.AskUvPointsContainment¶
-
Modeling.
AskUvPointsContainment
()¶ Refer to UF_MODL_ask_uv_points_containment for documentation.
Signature:
AskUvPointsContainment(nUvs, uParms, vParms, faceEid)
Parameters: - nUvs (int) – Number of 2D (u, v) points
- uParms (float) – Array of u parameters of 2D points
- vParms (float) – Array of v parameters of 2D points
- faceEid (Tag) – Face on which the 2D points are inquired
Returns: Array of the point containment status which have the following values: 1 = point is inside the face 2 = point is outside the face 3 = point is on the boundary of the face
Return type: list of int
License requirements: None