NXOpen.UF.Modeling.AskPointContainment¶
-
Modeling.
AskPointContainment
()¶ Refer to UF_MODL_ask_point_containment for documentation.
Signature:
AskPointContainment(point, body)
Parameters: - point (list of float) – Point coordinates of the inquiry point
- body (Tag) – Face, edge, solid, or sheet body tag onwhich point is inquired
Returns: Returned status of the point on the body 1 = point is inside the body 2 = point is outside the body 3 = point is on the body
Return type: int
License requirements: None