NXOpen.SIM.IsvControlPanelBuilder |
Represents a NXOpen.SIM.IsvControlPanelBuilder |
NXOpen.SIM.KinematicAxis |
Represents the SimKimAxis class object |
NXOpen.SIM.KinematicAxisBuilder |
Represents the SimKimAxisBuilder class object |
NXOpen.SIM.KinematicChain |
This class is used for add kinematic chain to the list. |
NXOpen.SIM.KinematicChainConfiguration |
This class is used for define kinematic chains. |
NXOpen.SIM.KinematicChainList |
Represents a list of objects. |
NXOpen.SIM.KinematicComponent |
Represents the KinematicComponent class object |
NXOpen.SIM.KinematicComponentBuilder |
Represents the KinamaticComponentBuilder class object |
NXOpen.SIM.KinematicComponentCollection |
Represents the SimKimComponent Collection |
NXOpen.SIM.KinematicConfigurator |
Represents the ISV base class object |
NXOpen.SIM.KinematicJunction |
Represents the KinematicJunction class object |
NXOpen.SIM.KinematicJunctionBuilder |
Represents the SimKimJunctionBuilder class object |
NXOpen.SIM.KinematicJunctionBuilderList |
Represents a list of objects. |
NXOpen.SIM.KinematicSinumerikCaBuilder |
This class is used for edit sinumerik collision avoidance properties. |
NXOpen.SIM.NcChannelSelectionData |
Represents the NcChannelSelectionData class object |
NXOpen.SIM.SinumerikCaExportBuilder |
This class is used for export a spf file. |
NXOpen.SIM.SinumerikCaFacetBuilder |
This class is used for set the facet tolerance. |
NXOpen.SIM.SinumerikCaPlaceholderBuilder |
This class is used for select or unselect component of the placeholder tools. |
NXOpen.SIM.SinumerikCaSimplifyBodiesBuilder |
This class is used for replace geometry. |