ScaleBuilder Class¶
-
class
NXOpen.Features.
ScaleBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.Scale
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateScaleBuilder
Default values.
Property Value ScaleAlongAxis.Value 1.0 ScaleOtherDirection.Value 1.0 ScaleXdirection.Value 1.0 ScaleYdirection.Value 1.0 ScaleZdirection.Value 1.0 UniformFactor.Value 1.0 New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BodyToScale | Returns the bodyToScale |
Csys | Returns or sets the csys as NXOpen.CoordinateSystem |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Point | Returns or sets the point as NXOpen.Point |
ScaleAlongAxis | Returns the scale along axis |
ScaleOtherDirection | Returns the scale other direction |
ScaleXdirection | Returns the scale xdirection |
ScaleYdirection | Returns the scale ydirection |
ScaleZdirection | Returns the scale zdirection |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the scale type NXOpen.Features.ScaleBuilderTypes |
UniformFactor | Returns the uniform factor |
Vector | Returns or sets the vector as NXOpen.Direction |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ScaleBuilderTypes Enumeration | Scale type |
Property Detail¶
BodyToScale¶
-
ScaleBuilder.
BodyToScale
¶ Returns the bodyToScale
-------------------------------------
Getter Method
Signature
BodyToScale()
Returns: Return type: NXOpen.SelectBodyList
New in version NX5.0.0.
License requirements: None.
Csys¶
-
ScaleBuilder.
Csys
¶ Returns or sets the csys as
NXOpen.CoordinateSystem
-------------------------------------
Getter Method
Signature
Csys()
Returns: Returns the reference Co-ordinate system from which scaling has to be done Return type: NXOpen.CoordinateSystem
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Csys(csys)
Parameters: csys ( NXOpen.CoordinateSystem
) – Set the reference Co-ordinate system from which scaling has to be doneNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Point¶
-
ScaleBuilder.
Point
¶ Returns or sets the point as
NXOpen.Point
-------------------------------------
Getter Method
Signature
Point()
Returns: Returns the referance point from which scaling has to be done Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) – Set the referance point from which scaling has to be doneNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ScaleAlongAxis¶
-
ScaleBuilder.
ScaleAlongAxis
¶ Returns the scale along axis
-------------------------------------
Getter Method
Signature
ScaleAlongAxis()
Returns: Scale factor along axis Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
ScaleOtherDirection¶
-
ScaleBuilder.
ScaleOtherDirection
¶ Returns the scale other direction
-------------------------------------
Getter Method
Signature
ScaleOtherDirection()
Returns: Scale factor along other direction Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
ScaleXdirection¶
-
ScaleBuilder.
ScaleXdirection
¶ Returns the scale xdirection
-------------------------------------
Getter Method
Signature
ScaleXdirection()
Returns: Scale factor along X Direction Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
ScaleYdirection¶
-
ScaleBuilder.
ScaleYdirection
¶ Returns the scale ydirection
-------------------------------------
Getter Method
Signature
ScaleYdirection()
Returns: Scale factor along Y Direction Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
ScaleZdirection¶
-
ScaleBuilder.
ScaleZdirection
¶ Returns the scale zdirection
-------------------------------------
Getter Method
Signature
ScaleZdirection()
Returns: Scale factor along Z Direction Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Type¶
-
ScaleBuilder.
Type
¶ Returns or sets the scale type
NXOpen.Features.ScaleBuilderTypes
-------------------------------------
Getter Method
Signature
Type()
Returns: Returns the type of the scale method Return type: NXOpen.Features.ScaleBuilderTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.ScaleBuilderTypes
) – Gets the type of the scale methodNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
UniformFactor¶
-
ScaleBuilder.
UniformFactor
¶ Returns the uniform factor
-------------------------------------
Getter Method
Signature
UniformFactor()
Returns: Uniform Scale factor Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Vector¶
-
ScaleBuilder.
Vector
¶ Returns or sets the vector as
NXOpen.Direction
-------------------------------------
Getter Method
Signature
Vector()
Returns: Returns the reference Axis along which scaling has to be done Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector(vector)
Parameters: vector ( NXOpen.Direction
) – Set the reference Axis along which scaling has to be doneNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
ScaleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.