CompositeBlock Class¶
-
class
NXOpen.BlockStyler.
CompositeBlock
¶ Bases:
NXOpen.BlockStyler.UIBlock
A composite block is a block that contains other blocks
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Cue | Returns or sets the Cue |
DialogSizing | Returns or sets the Dialog Sizing |
DialogSizingAsString | Returns or sets the Dialog Sizing as string |
Enable | Returns or sets the Enable. |
Expanded | Returns or sets the Expanded |
Group | Returns or sets the Group |
Label | Returns or sets the Label |
LastUpdated | Returns the block contained in the composite block that was last updated. |
Name | Returns the name of the block or BlockID |
NavigationStyle | Returns the Navigation Style |
NavigationStyleAsString | Returns the Navigation Style as string |
Show | Returns or sets the Visibility of block. |
Tag | Returns the Tag for this object. |
Type | Returns the type of block |
Methods¶
Method | Description |
---|---|
FindBlock | Finds a block contained in the composite block. |
Focus | Focuses on the block. |
GetBlocks | Gets all the blocks available in the composite block @return |
GetDialogSizingMembers | Gets the Dialog Sizing members @return Value to get from the property |
GetNavigationStyleMembers | Gets the Navigation Style members @return Value to get from the property |
GetProperties | Returns the properties of the block @return |
Property Detail¶
Cue¶
-
CompositeBlock.
Cue
¶ Returns or sets the Cue
-------------------------------------
Getter Method
Signature
Cue()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Cue(cue)
Parameters: cue (str) – New in version NX8.5.0.
License requirements: None.
DialogSizing¶
-
CompositeBlock.
DialogSizing
¶ Returns or sets the Dialog Sizing
-------------------------------------
Getter Method
Signature
DialogSizing()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DialogSizing(enumIndex)
Parameters: enumIndex (int) – New in version NX8.5.0.
License requirements: None.
DialogSizingAsString¶
-
CompositeBlock.
DialogSizingAsString
¶ Returns or sets the Dialog Sizing as string
-------------------------------------
Getter Method
Signature
DialogSizingAsString()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DialogSizingAsString(enumString)
Parameters: enumString (str) – New in version NX8.5.0.
License requirements: None.
LastUpdated¶
-
CompositeBlock.
LastUpdated
¶ Returns the block contained in the composite block that was last updated.
For example, if the CompositeBlock is an item contained in a SetList and your update handler is notified that the CompositeBlock has been updated, this method returns which block inside the CompositeBlock has been updated.
-------------------------------------
Getter Method
Signature
LastUpdated()
Returns: Return type: NXOpen.BlockStyler.UIBlock
New in version NX6.0.0.
License requirements: None.
Method Detail¶
FindBlock¶
-
CompositeBlock.
FindBlock
¶ Finds a block contained in the composite block.
Throws an exception if block not present
Signature
FindBlock(blockName)
Parameters: blockName (str) – Block name NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: NXOpen.BlockStyler.UIBlock
New in version NX6.0.0.
License requirements: None.
GetBlocks¶
-
CompositeBlock.
GetBlocks
¶ Gets all the blocks available in the composite block
Signature
GetBlocks()
Returns: Return type: list of NXOpen.BlockStyler.UIBlock
New in version NX6.0.0.
License requirements: None.