BlockDialogDialogMode Enumeration¶
NXOpen.BlockStyler.BlockDialog.DialogMode is an alias for NXOpen.BlockStyler.BlockDialogDialogMode
-
class
NXOpen.BlockStyler.
BlockDialogDialogMode
¶ Bases:
object
Datatype containing options for showing the dialog
Enum Members
dialog, the user’s inputs are saved in dialog memory and the next time that the dialog is shown in Create mode, the dialog is initialized using the user’s previous inputs. “
“Edit”, ” The Apply button is not shown.The user’s inputs are not saved in dialog memory and the dialog is not initialized with the user’s previous inputs. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-