Dimension Class¶
-
class
NXOpen.Annotations.
Dimension
¶ Bases:
NXOpen.Annotations.Annotation
,NXOpen.Annotations.IAppendedText
Represents a dimension
Abstract class
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
AnnotationOrigin | Returns or sets the origin (location) of the annotation. |
AnnotationPlane | Returns or sets the annotation plane. |
Color | Returns or sets the color of the object. |
ComputedSize | Returns the computed size of the dimension. |
HasAssociativeOrigin | Returns a flag indicating whether the origin is associative |
InspectionDimensionFlag | Returns or sets a setting to control the inspection box displayed around the dimension value. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsOriginCentered | Returns or sets a flag indicating whether the dimension text is centered equally between the extension lines. |
IsRetained | Returns a flag indicating whether the annotation is retained |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LeaderOrientation | Returns or sets the leader orientation for the annotation. |
LimitFitAnsiHoleType | Returns or sets the tolerance limit fit ANSI hole type. |
LimitFitDeviation | Returns or sets the tolerance limit fit deviation. |
LimitFitDisplayStyle | Returns or sets the tolerance limit fit display style. |
LimitFitEnhancedDisplayType | Returns or sets the enhanced limit fit display type. |
LimitFitGrade | Returns or sets the tolerance limit fit grade. |
LimitFitShaftDeviation | Returns or sets the deviation for limit fit representation of shaft tolerance NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. |
LimitFitShaftGrade | Returns or sets the grade for limit fit representation of shaft tolerance NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
LowerMetricToleranceValue | Returns or sets a setting to control the metric lower tolerance value of a dimension. |
LowerToleranceValue | Returns or sets a setting to control the lower tolerance value of a dimension. |
MeasurementDirection | Returns or sets the measurement direction. |
MeasurementDirectionView | Returns or sets the measurement direction view. |
MetricNominalDecimalPlaces | Returns or sets a setting to control the number of decimal places for the nominal value of a metric dimension. |
MetricToleranceDecimalPlaces | Returns or sets a setting to control the number of decimal places for the metric tolerance value of a dimension. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
NominalDecimalPlaces | Returns or sets a setting to control the number of decimal places for the nominal value of a dimension. |
NumberOfAssociativities | Returns the number of associativities for the annotation. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
ReferenceDimensionFlag | Returns or sets a setting to control the visibility of the reference parenthesis of a dimension. |
Tag | Returns the Tag for this object. |
ToleranceDecimalPlaces | Returns or sets a setting to control the number of decimal places for the primary tolerance value of a dimension. |
ToleranceType | Returns or sets a setting to control the tolerance display style. |
UpperMetricToleranceValue | Returns or sets a setting to control the metric upper tolerance value of a dimension. |
UpperToleranceValue | Returns or sets a setting to control the upper tolerance value of a dimension. |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAppendedText | Returns the appended text @return Appended text |
GetAssociativeOrigin | Gets data that specifies the origin’s associativity @return associativity data |
GetAssociativity | Returns the associativity at specified index. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDimensionPreferences | Returns the dimension preferences @return Dimenension preferences |
GetDimensionText | Returns the dimension text - both the main text and the dual text. |
GetFirstAssociativity | Returns the first associativity data. |
GetInferredAnnotationPlane | Returns the inferred annotation plane @return |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLetteringPreferences | Returns the lettering preferences for the annotation @return |
GetLineAndArrowPreferences | Returns the line and arrow preferences for the annotation @return |
GetMeasurementType | Returns dimension measurement type. |
GetNarrowDimensionPreferences | Returns the narrow dimension preferences for the given linear dimension. |
GetNarrowDimensionTextOffset | Returns the narrow dimension text offset for the given chain dimension. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSecondAssociativity | Returns the second associativity data. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetSymbolPreferences | Returns the symbol preferences for the annotation @return |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetViews | Returns the views that the PMI display instance object is displayed in NOTE: This method is only valid for PMI display instance objects. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Highlight | Highlights the object. |
InsertIntoStack | Inserts the annotation into a stack. |
IsApproximate | Returns whether or not the given dimension is approximate. |
IsDriving | Determines if a dimension is driving. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveViewDependency | Remove dependency on all views from an object. |
SetAppendedText | Sets the appended text |
SetAssociativeOrigin | Associates the annotation’s origin to the specified geometry. |
SetAssociativity | Sets the associativity at specified index. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetComputedSize | |
SetDimensionPreferences | Sets the dimension preferences |
SetDimensionText | Set the main dimension text. |
SetFirstAssociativity | Sets the first associativity data. |
SetLetteringPreferences | Sets the lettering preferences for the annotation. |
SetLineAndArrowPreferences | Sets the line and arrow preferences for the annotation. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetNarrowDimensionPreferences | Sets the narrow dimension preferences to the given linear dimension. |
SetNarrowDimensionTextOffset | Sets the narrow dimension text offset for the given chain dimension. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSecondAssociativity | Sets the second associativity data. |
SetSymbolPreferences | Sets the symbol preferences for the annotation. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetViews | Sets the views that the PMI display instance object is displayed in. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Enumerations¶
DimensionMeasurementTypes Enumeration | Specifies dimension measurement types |
Property Detail¶
ComputedSize¶
-
Dimension.
ComputedSize
¶ Returns the computed size of the dimension.
-------------------------------------
Getter Method
Signature
ComputedSize()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
InspectionDimensionFlag¶
-
Dimension.
InspectionDimensionFlag
¶ Returns or sets a setting to control the inspection box displayed around the dimension value.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
InspectionDimensionFlag()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InspectionDimensionFlag(inspectionDimensionFlag)
Parameters: inspectionDimensionFlag (bool) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
IsOccurrence¶
-
Dimension.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
IsOriginCentered¶
-
Dimension.
IsOriginCentered
¶ Returns or sets a flag indicating whether the dimension text is centered equally between the extension lines.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
IsOriginCentered()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsOriginCentered(isOriginCentered)
Parameters: isOriginCentered (bool) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
JournalIdentifier¶
-
Dimension.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
LimitFitAnsiHoleType¶
-
Dimension.
LimitFitAnsiHoleType
¶ Returns or sets the tolerance limit fit ANSI hole type.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
LimitFitAnsiHoleType()
Returns: Limit fit ansi hole type Return type: NXOpen.Annotations.FitAnsiHoleType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitFitAnsiHoleType(fitHoleType)
Parameters: fitHoleType ( NXOpen.Annotations.FitAnsiHoleType
) – New limit fit ansi hole typeNew in version NX7.5.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LimitFitDeviation¶
-
Dimension.
LimitFitDeviation
¶ Returns or sets the tolerance limit fit deviation.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
LimitFitDeviation()
Returns: Limit fit deviation Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitFitDeviation(fitDeviation)
Parameters: fitDeviation (str) – New limit fit deviation New in version NX7.5.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LimitFitDisplayStyle¶
-
Dimension.
LimitFitDisplayStyle
¶ Returns or sets the tolerance limit fit display style.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
LimitFitDisplayStyle()
Returns: Limit fit tolerance display style Return type: NXOpen.Annotations.FitDisplayStyle
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitFitDisplayStyle(fitDisplayStyle)
Parameters: fitDisplayStyle ( NXOpen.Annotations.FitDisplayStyle
) – New limit fit tolerance display styleNew in version NX7.5.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LimitFitEnhancedDisplayType¶
-
Dimension.
LimitFitEnhancedDisplayType
¶ Returns or sets the enhanced limit fit display type.
Used to determine if the tolerance representation is for hole, shaft, or fit tolerance (fit meaning both hole and shaft tolerances are displayed).
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
LimitFitEnhancedDisplayType()
Returns: Limit fit enhanced tolerance display style Return type: NXOpen.Annotations.FitAnsiHoleType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitFitEnhancedDisplayType(fitEnhancedDisplayType)
Parameters: fitEnhancedDisplayType ( NXOpen.Annotations.FitAnsiHoleType
) – New limit fit enhanced tolerance display styleNew in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LimitFitGrade¶
-
Dimension.
LimitFitGrade
¶ Returns or sets the tolerance limit fit grade.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
LimitFitGrade()
Returns: Limit fit grade Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitFitGrade(fitGrade)
Parameters: fitGrade (int) – New limit fit grade New in version NX7.5.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LimitFitShaftDeviation¶
-
Dimension.
LimitFitShaftDeviation
¶ Returns or sets the deviation for limit fit representation of shaft tolerance
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
LimitFitShaftDeviation()
Returns: Limit fit shaft deviation Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitFitShaftDeviation(fitShaftDeviation)
Parameters: fitShaftDeviation (str) – New limit fit shaft deviation New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LimitFitShaftGrade¶
-
Dimension.
LimitFitShaftGrade
¶ Returns or sets the grade for limit fit representation of shaft tolerance
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
LimitFitShaftGrade()
Returns: Limit fit shaft grade Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitFitShaftGrade(fitShaftGrade)
Parameters: fitShaftGrade (int) – New limit fit shaft grade New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LowerMetricToleranceValue¶
-
Dimension.
LowerMetricToleranceValue
¶ Returns or sets a setting to control the metric lower tolerance value of a dimension.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
LowerMetricToleranceValue()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerMetricToleranceValue(toleranceValue)
Parameters: toleranceValue (float) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LowerToleranceValue¶
-
Dimension.
LowerToleranceValue
¶ Returns or sets a setting to control the lower tolerance value of a dimension.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
LowerToleranceValue()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerToleranceValue(upperToleranceValue)
Parameters: upperToleranceValue (float) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
MeasurementDirection¶
-
Dimension.
MeasurementDirection
¶ Returns or sets the measurement direction.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
MeasurementDirection()
Returns: Direction Object Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeasurementDirection(direction)
Parameters: direction ( NXOpen.Direction
) – Direction ObjectNew in version NX7.5.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
MeasurementDirectionView¶
-
Dimension.
MeasurementDirectionView
¶ Returns or sets the measurement direction view.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
MeasurementDirectionView()
Returns: View Object Return type: NXOpen.View
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeasurementDirectionView(view)
Parameters: view ( NXOpen.View
) – View ObjectNew in version NX7.5.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
MetricNominalDecimalPlaces¶
-
Dimension.
MetricNominalDecimalPlaces
¶ Returns or sets a setting to control the number of decimal places for the nominal value of a metric dimension.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
MetricNominalDecimalPlaces()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MetricNominalDecimalPlaces(decimalPlaces)
Parameters: decimalPlaces (int) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
MetricToleranceDecimalPlaces¶
-
Dimension.
MetricToleranceDecimalPlaces
¶ Returns or sets a setting to control the number of decimal places for the metric tolerance value of a dimension.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
MetricToleranceDecimalPlaces()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MetricToleranceDecimalPlaces(decimalPlaces)
Parameters: decimalPlaces (int) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Name¶
-
Dimension.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
NominalDecimalPlaces¶
-
Dimension.
NominalDecimalPlaces
¶ Returns or sets a setting to control the number of decimal places for the nominal value of a dimension.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
NominalDecimalPlaces()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NominalDecimalPlaces(decimalPlaces)
Parameters: decimalPlaces (int) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
OwningComponent¶
-
Dimension.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Dimension.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Dimension.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
ReferenceDimensionFlag¶
-
Dimension.
ReferenceDimensionFlag
¶ Returns or sets a setting to control the visibility of the reference parenthesis of a dimension.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
ReferenceDimensionFlag()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceDimensionFlag(referenceDimensionFlag)
Parameters: referenceDimensionFlag (bool) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ToleranceDecimalPlaces¶
-
Dimension.
ToleranceDecimalPlaces
¶ Returns or sets a setting to control the number of decimal places for the primary tolerance value of a dimension.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
ToleranceDecimalPlaces()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToleranceDecimalPlaces(decimalPlaces)
Parameters: decimalPlaces (int) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ToleranceType¶
-
Dimension.
ToleranceType
¶ Returns or sets a setting to control the tolerance display style.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
ToleranceType()
Returns: Return type: NXOpen.Annotations.ToleranceType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToleranceType(toleranceType)
Parameters: toleranceType ( NXOpen.Annotations.ToleranceType
) –New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
UpperMetricToleranceValue¶
-
Dimension.
UpperMetricToleranceValue
¶ Returns or sets a setting to control the metric upper tolerance value of a dimension.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
UpperMetricToleranceValue()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperMetricToleranceValue(toleranceValue)
Parameters: toleranceValue (float) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
UpperToleranceValue¶
-
Dimension.
UpperToleranceValue
¶ Returns or sets a setting to control the upper tolerance value of a dimension.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
UpperToleranceValue()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperToleranceValue(upperToleranceValue)
Parameters: upperToleranceValue (float) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Method Detail¶
FindObject¶
-
Dimension.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAppendedText¶
-
Dimension.
GetAppendedText
¶ Returns the appended text
Signature
GetAppendedText()
Returns: Appended text Return type: NXOpen.Annotations.AppendedText
New in version NX4.0.0.
License requirements: None.
GetDimensionPreferences¶
-
Dimension.
GetDimensionPreferences
¶ Returns the dimension preferences
Signature
GetDimensionPreferences()
Returns: Dimenension preferences Return type: NXOpen.Annotations.DimensionPreferences
New in version NX4.0.0.
License requirements: None.
GetDimensionText¶
-
Dimension.
GetDimensionText
¶ Returns the dimension text - both the main text and the dual text.
The returned text may contain just the computed dimension value or manual text including the control characters.
Note that the text doesn’t contain the tolerance text, appended text or text for flags like inspection/reference.
Signature
GetDimensionText()
Returns: a tuple Return type: A tuple consisting of (mainTextLines, dualTextLines). mainTextLines is a list of str. List of main text lines dualTextLines is a list of str. List of dual text lines New in version NX6.0.0.
License requirements: None.
GetFirstAssociativity¶
-
Dimension.
GetFirstAssociativity
¶ Returns the first associativity data.
Signature
GetFirstAssociativity()
Returns: Return type: NXOpen.Annotations.Associativity
New in version NX5.0.0.
License requirements: None.
GetMeasurementType¶
-
Dimension.
GetMeasurementType
¶ Returns dimension measurement type.
Signature
GetMeasurementType()
Returns: Dimension Measurement Type. Return type: NXOpen.Annotations.DimensionMeasurementTypes
New in version NX10.0.0.
License requirements: None.
GetNarrowDimensionPreferences¶
-
Dimension.
GetNarrowDimensionPreferences
¶ Returns the narrow dimension preferences for the given linear dimension.
Signature
GetNarrowDimensionPreferences()
Returns: Narrow dimension preferences Return type: NXOpen.Annotations.NarrowDimensionData
New in version NX5.0.0.
License requirements: None.
GetNarrowDimensionTextOffset¶
-
Dimension.
GetNarrowDimensionTextOffset
¶ Returns the narrow dimension text offset for the given chain dimension.
Signature
GetNarrowDimensionTextOffset()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
GetSecondAssociativity¶
-
Dimension.
GetSecondAssociativity
¶ Returns the second associativity data.
Signature
GetSecondAssociativity()
Returns: Return type: NXOpen.Annotations.Associativity
New in version NX5.0.0.
License requirements: None.
IsApproximate¶
-
Dimension.
IsApproximate
¶ Returns whether or not the given dimension is approximate.
A dimension is approximate if it is attached to lightweight view geometry that doesn’t have exact data.
Signature
IsApproximate()
Returns: TRUE, if dimension is approximate. FALSE, if dimension is not approximate. :rtype: bool
New in version NX9.0.0.
License requirements: None.
IsDriving¶
-
Dimension.
IsDriving
¶ Determines if a dimension is driving.
A driving dimension is a dimension that is used to constrain geometry created by the sketcher on a drawing. A driving dimension is also referred to as a sketch dimension.
Signature
IsDriving()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
Print¶
-
Dimension.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetAppendedText¶
-
Dimension.
SetAppendedText
¶ Sets the appended text
Signature
SetAppendedText(appendedText)
Parameters: appendedText ( NXOpen.Annotations.AppendedText
) – Appended textNew in version NX4.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SetComputedSize¶
-
Dimension.
SetComputedSize
¶ Signature
SetComputedSize(computedSize)
Parameters: computedSize (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Use
Annotations.Dimension.SetDimensionText
instead.License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SetDimensionPreferences¶
-
Dimension.
SetDimensionPreferences
¶ Sets the dimension preferences
Signature
SetDimensionPreferences(preferences)
Parameters: preferences ( NXOpen.Annotations.DimensionPreferences
) – New dimension preferencesNew in version NX4.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SetDimensionText¶
-
Dimension.
SetDimensionText
¶ Set the main dimension text.
For a dual dimension, the dual dimension text is determined from the main dimension text
Signature
SetDimensionText(mainTextLines)
Parameters: mainTextLines (list of str) – List of main text lines New in version NX7.5.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SetFirstAssociativity¶
-
Dimension.
SetFirstAssociativity
¶ Sets the first associativity data.
Signature
SetFirstAssociativity(newAssociativity)
Parameters: newAssociativity ( NXOpen.Annotations.Associativity
) –New in version NX5.0.0.
License requirements: None.
SetName¶
-
Dimension.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetNarrowDimensionPreferences¶
-
Dimension.
SetNarrowDimensionPreferences
¶ Sets the narrow dimension preferences to the given linear dimension.
Signature
SetNarrowDimensionPreferences(narrowDimensionData)
Parameters: narrowDimensionData ( NXOpen.Annotations.NarrowDimensionData
) – New narrow dimension preferencesNew in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SetNarrowDimensionTextOffset¶
-
Dimension.
SetNarrowDimensionTextOffset
¶ Sets the narrow dimension text offset for the given chain dimension.
Signature
SetNarrowDimensionTextOffset(narrowTextOffset)
Parameters: narrowTextOffset (float) – New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SetSecondAssociativity¶
-
Dimension.
SetSecondAssociativity
¶ Sets the second associativity data.
Signature
SetSecondAssociativity(newAssociativity)
Parameters: newAssociativity ( NXOpen.Annotations.Associativity
) –New in version NX5.0.0.
License requirements: None.