Overview | Statement List | Example
CROSSF(vector1,vector2)
Returns the cross product of two vectors. Using the function as shown below, where A and B are arrays, each consisting of the three components of a vector,
NUMBER/A(3),B(3),C(3)
C=CROSSF(A,B)
is equivalent to the following expressions:
C(1) = A(2)*B(3)-A(3)*B(2)
C(2) = -(A(1)*B(3)-A(3)*B(1))
C(3) = A(1)*B(2)-A(2)*B(1)
Parameter |
Description |
vector1,vector2 |
Two-, three-position numerical arrays which represents the components of vectors. |