Testing dashboard
This dashboard provides a view on the current state of unit test coverage and success ratio of unit tests. It also provides drill-down links to details about coverage and to your unit tests. It shows unit test success ratio and coverage for Maven artifacts with Java sources and tests. The detailed Maven unit test and coverage reports are linked.
Data shown in this topic are updated either during the Process Audit calculation (processaudit) or when the artifact is built using the option Update reports together with the build.
For more information, see Complex and Custom Building.
Testing statistics and drill-down from the Testing dashboard.