Terminology
The following terminology is used in the Polarion VARIANTS documentation.
Polarion VARIANTS Glossary
Features | Components of a product, whether they are hardware, software, or other functionality needed. When capitalized in documentation, Work Items of type "Feature". |
Feature Model | Describes every possible feature of a product line. It is where a company can model their product line by decomposing all products to see what they have in common and what parts differ. Then, they assign functionality to features. |
Master Specification | A Polarion Document containing all possible artifacts of one or more types for a Product Line, for example, all Requirements or all Test Cases. Each artifact is linked to one or more Features in the Feature Model. A Variant Specification contains a subset of the artifacts from a Master Specification. Master Specifications can be as granular as needed. For example, you can have Master Specifications for Functional, Non-functional, and System Requirements. |
Product Line | Also called product family, it is the collection of all products a company produces. The different products may have some common components that must be in every product and some components that differ from product to product. |
Relation | Links between Features that denote additional relationships depending on the link type. For example:
|
Restriction | A property of Work Items in a Master Specification that sets certain restriction(s) or limits on the item's inclusion in Variants. Specified in pvSCL (the restriction language of the Pure Systems back end), for example: Feature1 AND Not(Feature2). |
Validation | Checks by the Polarion VARIANTS back end to ensure that variants contain only valid assets and information. There are two types of Validation checks:
|
Variation Type | A property of a Feature that describes the Feature's inclusion in product specifications. A feature can have one of four Variation Types:
|
Variant | When capitalized, a Work Item type that collects Features and assets from Master Specifications to fully describe a specific product in the Product Line. This type is predefined in Polarion project templates with variant management support. When not capitalized, denotes one specific product in a Product Line, for example, "Model ABC is a variant of the WeatherStation product line". |
Variant Description Model (VDM) | Assets, such as Requirements and Test Cases, that are mapped to Features that collectively make up a Variant |
Variant Specification | A specification Document generated from a Variant and comprised of commonalities and variations from the Feature Model and Master Specification. |